Position_window_time
Index.Sub | |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable | No |
Unit |
milliseconds (ms) |
Range |
Unsigned16 |
Default Value | 0 |
Store Supported | No |
Description | When the actual position is within the Position_window during the defined position window time, the corresponding bit10 target reached in the Statusword will be set to one. |
Notes |
-- |